Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Load Options Configuration Context "Load As Saved"

Creator
Creator

Can someone explain to me what the "Load As Saved" in the Assembly Load Options Configuration Context is doing? This option appears when using NX with TeamCenter. I've searched within the NX help and can not find any information.

 

Thank you

Matt 

6 REPLIES

Re: Assembly Load Options Configuration Context "Load As Saved"

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
It loads the structure as it was last saved in the NX part file, rather than from the BVR in Teamcenter.

Regards, Ben

Re: Assembly Load Options Configuration Context "Load As Saved"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I.e. if you saved an assembly with component A at revision 1 (already released)

Now someone updates "A" to revision 2, then releases it

Then someone updates "A" to rev 3, but does not release it

 

Load as saved will open rev 1 of "A"

Load latest released will open rev 2

Load latest working will load rev 3

 

Or something like that.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Assembly Load Options Configuration Context "Load As Saved"

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
And then there's Precise/Imprecise... but I'll leave that for another day.

Ben

Re: Assembly Load Options Configuration Context "Load As Saved"

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Here's the documentation regarding Load As Saved:

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:xid611298

"The assembly is loaded with the revision rule load options that were specified when the assembly was saved. This allows you to load the assembly with the revision instances as it was last saved."

Re: Assembly Load Options Configuration Context "Load As Saved"

Creator
Creator

@BenBroad wrote:
It loads the structure as it was last saved in the NX part file, rather than from the BVR in Teamcenter.

Regards, Ben


That's what I thought! A coworker was explaining this "Load As Saved" option to me and what I gathered was that this "Load As Saved" was for the load option saved default file. So when I opened a NX file with this option selected, it would use the load option saved default file tha I may have saved. Maybe I miss understood what he was saying. I could not see how this would work, becasue if the "Load As Saved" was in the saved default file, it would create a loop.


 Thanks for your help!

 

Matt

Re: Assembly Load Options Configuration Context "Load As Saved"

Creator
Creator

@BenBroad wrote:
And then there's Precise/Imprecise... but I'll leave that for another day.

Ben

I'm trying to understand the load options in NX with TC and eventually get to the Precise and Imprecise.