Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Assembly constraints, Next higher level references possible?

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @s_hightower

 

You might also want to look into using the Product Interface functionality:

 

Useful product interfaces include the following:

  • Faces that should be used for mating when you add your part as a component to an assembly.

 

(view in My Videos)

 

Regards, Ben

Re: Assembly constraints, Next higher level references possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Another reason it may not show up is if you don't have the "Assemblies" application chosen (in the "Applications" ribbon tab - it should have a different color background than the rest of the ribbon bar background)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Assembly constraints, Next higher level references possible?

Genius
Genius

Thanks, everyone, for the info.  After knowing where to look, I was able to find the override position option.  I'll have to look a the instructions for that and try working with it.  I'll also need to review the product interface info.  Thanks, again.  I do appreciate the help.