Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Assembly

Experimenter
Experimenter

Hi, is it possible, with nx, to save an assembly as a single part?

2 REPLIES

Re: Assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @FrancescoB_1968,

You can do 'File > Export > Part' and use the available options so that all geometry will be exported in a single part with options to remove/retain the feature parameters.

Export Part dialog box

Re: Assembly

Valued Contributor
Valued Contributor

For an assemblie you can use EXPORT -- PARASOLID, than open an new empty part and import the parasolid file. You get the same geometrie without an assemblie structure and without features.

Wolfgang