Cancel
Showing results for 
Search instead for 
Did you mean: 

Assign correct crosshatch to material

Phenom
Phenom

Hi,

someone know a workaround to assign the correct crosshatch when assign material to part ?

When I create a section view in drawing the crosshatch is always 'Iron' independent if the part is aluminum or rubber.

When I create section view in drawing for assembly the problem is more visible.

Another question ....it's possible to assign a different crosshatch value for weld feature, so when I create section view, sectioned weld are with a crosshatch like was filled ?  

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

4 REPLIES

Re: Assign correct crosshatch to material

Siemens Phenom Siemens Phenom
Siemens Phenom

If you're using the Material library, the cross hatch pattern is defined by the material so should be OK. Example below:

 

Library Material : Aluminum_2014
Category METAL
Library Reference physicalmateriallibrary.xml
Category : METAL
Sub-Category : Aluminum Alloy
Mass Density (RHO) : 2.794e-06kg/mm³
...
...
======== Miscellaneous
Crosshatch Pattern : Aluminum/Magnesium

 

If you have your own material defined, check the Visual Properties in the Miscellaneous section .

 

Dave

Re: Assign correct crosshatch to material

Phenom
Phenom

Hi @Dave_Walker,

after assigned the material with this new modification, the section view in drawing remain represented with 'iron' crosshatch. This solution works on PMI 3D section, not on drawing.

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: Assign correct crosshatch to material

Siemens Phenom Siemens Phenom
Siemens Phenom

Oh, OK.  @cubalibre00 I'll let the drafting experts chime in then Smiley Happy.

 

Dave

Re: Assign correct crosshatch to material

Valued Contributor
Valued Contributor

Hi,

 

Reply to question 1: In the view Settings > Section > Settings > turn off 'Process Hidden Crosshatch', now try to edit the Crosshatch by double clickling the available crosshatch.

 

Reply to question 2: Menu > Insert > Annotation > Crosshatch

 

As far as I know there no automatic inheritance of crosshatch in Drafting for the applied material.

.chx files present in UGII_UTIL directory will appear in Drafting 

 

 

 

-Santhosh