Cancel
Showing results for 
Search instead for 
Did you mean: 

Assign material to part without body

Legend
Legend

Is it possible to assign material to part without solid body?

There are some cases when we have parts which dont have solid body and we need to have material attribute for them seems like GLUE or MASTIC.

 

The Assign Material option in NX assign material for part with solid body only

13 REPLIES 13
Highlighted

Re: Assign material to part without body

Experimenter
Experimenter

You can assign a material to a sheet body, will that not help?

 

Failing that create a body and hide it or put it on a non-displayed layer maybe?

Re: Assign material to part without body

Legend
Legend

@Paul_Nissan wrote:

You can assign a material to a sheet body, will that not help?

 

Failing that create a body and hide it or put it on a non-displayed layer maybe?


May be it's a good idea. I'll make consultations with chiefs

Re: Assign material to part without body

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
If you use a solid body assign there the material to and the exclude it from a reference set So the solid wont be on the drawing.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Assign material to part without body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Would using a solid (vs. a sheet) affect assembly weight calculations?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Assign material to part without body

Honored Contributor
Honored Contributor

Can the "Material" or "NX_Material" (depending on NX version) attribute be written, without a body to assign it to?  maybe via a program of some sort?

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: Assign material to part without body

Legend
Legend

@DaveK wrote:

Can the "Material" or "NX_Material" (depending on NX version) attribute be written, without a body to assign it to?  maybe via a program of some sort?


I tried. No succsess.The solid body required.

Re: Assign material to part without body

Siemens Phenom Siemens Phenom
Siemens Phenom

What if you go with @ruud_vandenbrand's suggestion?

One other way could be, Just add a simple block > Assign Material > Delete the block with "Delete Body" command. There will be no solid body in the part, weight will be zero and material attribute will remain.

Re: Assign material to part without body

Legend
Legend

@ganesh_Kadole wrote:

What if you go with @ruud_vandenbrand's suggestion?

One other way could be, Just add a simple block > Assign Material > Delete the block with "Delete Body" command. There will be no solid body in the part, weight will be zero and material attribute will remain.


If I delete body the Material attribute value also deleting

Re: Assign material to part without body

Siemens Phenom Siemens Phenom
Siemens Phenom


If I delete body the Material attribute value also deleting


Did you use 'Delete Body' command or simply Delete?


matbody.png