Cancel
Showing results for 
Search instead for 
Did you mean: 

Associated Geometry with PMI

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Good Morning,

 

We're moving along well with PMI but it's still a little slow. We are right now stuck on a few minor things when creating PMI.

 

In PMI, we can select the Associated Objects; surfaces, edges, cylinders, etc. We can continue to select features but it seems we can't remove or delete them. Is there a way to edit this selection and remove features? Or edit the selected features?

 

Thanks,

Jason

1 REPLY

Re: Associated Geometry with PMI

Siemens Phenom Siemens Phenom
Siemens Phenom

During selection of the associated objects, you can deselect any errant pick by holding down the Shift key and reselecting the object.

 

After a PMI object is created, you can highlight it in the PMI group in the Part Navigator, Right-click and select 'Edit'.

 

Then, make the 'Associated Objects' icon active, and deselect the undesired objects.