Cancel
Showing results for 
Search instead for 
Did you mean: 

Associative Pattern For Object

Experimenter
Experimenter

Hello,

 

My name is Gualda and I have a question about NX10. I have an object and I would like to do and associative pattern following a matrix or a datum. Firstly what I have tried is to do directly a Copy, but it doesn’t have the possibility to be associative which the first object, which should be the master. I show in the next picture P_1.

 P_1.png

Also I have tryed creating a featured group and using featured pattern, but it also affected to the original object, chaning the geometry as you can see in picture P_2.

 P_2.jpg

There isnt any comand special for object?

 

Thanks!!!

1 REPLY 1

Re: Associative Pattern For Object

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @ncgualda,

 

Have you looked at "Menu > Insert > Associative Copy > Pattern Geometry"?  Set the Layout option to Circular, define your vector and rotation point and enter your Count and Pitch Angle.  This should give you an associative copy of your geometry.

Screenshot - 3_21_2018 , 11_26_31 AM.png

 

Regards, Ben