Cancel
Showing results for 
Search instead for 
Did you mean: 

Associative Pattern For Object

Experimenter
Experimenter

Hello,

 

My name is Gualda and I have a question about NX10. I have an object and I would like to do and associative pattern following a matrix or a datum. Firstly what I have tried is to do directly a Copy, but it doesn’t have the possibility to be associative which the first object, which should be the master. I show in the next picture P_1.

 P_1.png

Also I have tryed creating a featured group and using featured pattern, but it also affected to the original object, chaning the geometry as you can see in picture P_2.

 P_2.jpg

There isnt any comand special for object?

 

Thanks!!!

2 REPLIES 2

Re: Associative Pattern For Object

Valued Contributor
Valued Contributor

Hello @ncgualda,

 

As i understood, you looking for a pattern/mirror command with associative option, right? If so you looking for ''Pattern Geometry'' and ''Mirror Geometry'' command. Take a look the command settings; you will see ''Associative'' option. (pic1, pic2 is at below).

 

Hope it works, have a nice day.

 

2.png3.png

 

 

Re: Associative Pattern For Object

Experimenter
Experimenter

Thanks, it was exactly what I needed! Smiley Happy