Cancel
Showing results for 
Search instead for 
Did you mean: 

AutoTrace in NX?

Genius
Genius
"Autotrace will convert geometry from an image to a sketch."
 
I wonder whether there is similar functionality in NX.
 
Thanks!
7 REPLIES 7

Re: AutoTrace in NX?

Legend
Legend

No there isn't.

 

When I have to do this, I either bring the image in and sketch over it or if it is a vector based PFD I'll use the method.

 

https://nirklars.wordpress.com/2015/04/22/pdf-to-dwg-using-free-open-source-inkscape/

 

VectorMagic is pretty slick as well if you have a few to do, you can use it by the month fairly cheap.

 

 

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: AutoTrace in NX?

Genius
Genius

Hi @R_Newcomb  Thank you for sharing your solutions!

Re: AutoTrace in NX?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Video is bit old but theory is the same, it explains how to use Inkscape with NX: https://vimeo.com/83654051

Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: AutoTrace in NX?

Genius
Genius

Hi @PhoeNX_Support   Thank you for sharing the video!

Re: AutoTrace in NX?

Siemens Phenom Siemens Phenom
Siemens Phenom

Anthony,

I was about to mention the videos that Phoenx PLM has published when i saw your post.

-you guys make wonderful videos, this tip on Inkscape is how I handle raster conversions.

- but please skip the music...

 

( btw, notice in the how to guide for "that other system" how poor the quality is on the final sketch..)

 

Best regards,
 Tomas

Highlighted

Re: AutoTrace in NX?

Siemens Phenom Siemens Phenom
Siemens Phenom

One more option is to use Win Topo similar to Inkspace, Vector Magic.

Re: AutoTrace in NX?

Genius
Genius

Hi @GaneshKadole  Thanks for sharing!