03-28-2017 03:43 PM
Where did they move the option to run off automatic centerlines, in the Customer Defaults?
Solved! Go to Solution.
03-28-2017 04:17 PM
Hi Dave,
Menu -> File -> Utilities -> Customer Defaults...
Use the Search Function (binoculars icon) up un the right corner of the Customer Defaults menu that pops up
Search for "Create With Centerline"
03-28-2017 04:29 PM - edited 03-28-2017 04:37 PM
Should have figured the terminology would change, so that my endless searches, and searching would fail. *EDIT* I swear it was called "automatic centerlines" in the past, but looking at NX9 native, it simply says "centerlines".
I suppose I have to go thru all of my drafting formats now too, since the setting terminology has changed, to turn it back of in them?