Cancel
Showing results for 
Search instead for 
Did you mean: 

Automation of parametric model

Experimenter
Experimenter

Hello

 

I am planning to develop a parametric wing model using NX. The idea is to use programming to achieve automatic creation & update of the model geometry and mesh pattern (pre-processing of FE), which is expected to facilitate my structural optimisation work.

 

I am wondering are there any specific tools/options available in NX which can achieve this objective? Or what are the common methods that NX users usually apply for this kind of task?

 

Many thanks

 

Chao

1 REPLY 1
Highlighted

Re: Automation of parametric model

Siemens Phenom Siemens Phenom
Siemens Phenom
I have seen a demo of such a "piece", I think it was built using Knowledge Fusion , which is a "programming language" in NX.
You can probably use any programming language which "hooks into NX".

The case i saw was to optimize the cold shape of jet engine turbine blades such that the hot, working shape, should be optimal.

Regards,
Tomas