Cancel
Showing results for 
Search instead for 
Did you mean: 

Autoorder of dimensions

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello  everyone!

 

How I can make autodimenssions and  autoorder of dimensions in NX in draft? 

 

best regards

Lukipap

6 REPLIES 6

Re: Autoorder of dimensions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

you can take some help from FEATURE PARAMETERS for autodimension (not all features but still ...)

211.jpg

 

 

For auto order (distributing it properly) use DISTRIBUTE ANNOTATIONS.

222.jpg

 

Regards

Kapil

Re: Autoorder of dimensions

Phenom
Phenom

Hi,

the command 'DISTRIBUTE ANNOTATIONS' is found but not available ?

I've lost some news ?

DISTRIBUTE ANNOTATIONS.png

Thank you...

Using NX1859
RuleDesigner PDM

Re: Autoorder of dimensions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 I can access it and use it also in NX11.0.2.

DSS.jpg

 

Best Regards

Kapil

Re: Autoorder of dimensions

Phenom
Phenom

Hi @kapilsharma,

if you see the command and me not, then this command is under special license like Drawing Automation.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Autoorder of dimensions

Siemens Phenom Siemens Phenom
Siemens Phenom

Smiley Happy yes i guess that is correct (lmtools also directs in that direction) ...

Probably a drafting expert can throw some more light on it.

Best Regards

Kapil

Highlighted

Re: Autoorder of dimensions

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @cubalibre00,

 

You need a license increment called "nx_drawing_auto". From what I'm reading it looks like this is available in the following three bundles:

 

NX30130 - Drafting Plus
NX30173 - Drawing Automation for NX
NX10105 - NX Mach Power Drafting

 

Regards, Ben