05-17-2017 04:50 AM - edited
Hello everyone!
How I can make autodimenssions and autoorder of dimensions in NX in draft?
best regards
Lukipap
05-17-2017 05:25 AM
Hi,
you can take some help from FEATURE PARAMETERS for autodimension (not all features but still ...)
For auto order (distributing it properly) use DISTRIBUTE ANNOTATIONS.
Regards
Kapil
08-29-2017 03:22 AM
Hi,
the command 'DISTRIBUTE ANNOTATIONS' is found but not available ?
I've lost some news ?
08-29-2017 03:37 AM
Hi,
I can access it and use it also in NX11.0.2.
Best Regards
Kapil
08-29-2017 03:42 AM
Hi @kapilsharma,
if you see the command and me not, then this command is under special license like Drawing Automation.
08-29-2017 03:51 AM
yes i guess that is correct (lmtools also directs in that direction) ...
Probably a drafting expert can throw some more light on it.
Best Regards
Kapil
08-29-2017 11:37 AM
Hi @cubalibre00,
You need a license increment called "nx_drawing_auto". From what I'm reading it looks like this is available in the following three bundles:
NX30130 - Drafting Plus
NX30173 - Drawing Automation for NX
NX10105 - NX Mach Power Drafting
Regards, Ben