Cancel
Showing results for 
Search instead for 
Did you mean: 

Balloon headers in drawings NX 11 ?

Genius
Genius

Hello

I'm trying to replicate the balloons on left picture.

1.) How to make off-set leaders that are not locked to a certain line on part ?

2.) How to make a balloon without no dividing branch = leaders start from the balloon ?

 

measures.jpg

3 REPLIES 3

Re: Balloon headers in drawings NX 11 ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444,

In the balloon dialog -

1) Under Leader - List group toggle off option 'Apply Style Settings to All'

2) Create first leader with stub side on left

3) Create second leader with stub side on right

 

Balloon_Settings.png

Re: Balloon headers in drawings NX 11 ?

Siemens Legend Siemens Legend
Siemens Legend

Select the option , Without stub.

Then the rest is automatic.

 

In older versions of NX, one set the "stub length" to 0, but newer versions has this option "without stub".

 

 

image.png

 

Regards,

 Tomas

Re: Balloon headers in drawings NX 11 ?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @12131444,

 

1.) How to make off-set leaders that are not locked to a certain line on part ?

 


If you're using the Autoballoon functionality, you cannot have the system terminate the leaders on faces of components - it will only use the edge curves of the components.

 

ER 1815564 - Cannot define faces as terminating object while creating auto ballons.

 

Having selected Autoballoon, right click a leader and choose Edit.  Pick the location on the face of the component where you want to terminate the leader and then close the Balloon dialog.  The annotation in the balloon will remain associative to the Parts List.

 

Regards, Ben