Cancel
Showing results for 
Search instead for 
Did you mean: 

Balloon size must be larger than 0

Master
Master

When in drafting I try to use a balloon with arrow and get this error. I checked preferences and it is set to 14. What is up with that? LOL

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
4 REPLIES 4

Re: Balloon size must be larger than 0

Valued Contributor
Valued Contributor

I had the same problem today, I terminated the NX Session and then  deleted %USERPROFILE%\AppData\Local\Siemense\NX110\DialogMemory.dlx file. 

When I started a new Session the problem disappeared. 

Re: Balloon size must be larger than 0

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Here's an FAQ on the same issue:

Inserting ID symbol causes error  "Balloon size must be greater than zero."

 

A similar issue was reported in PR 8969636.  I was possible to enter a very small value for the balloon size, that NX interpreted as zero when the dialog was reopened (due to dialog memory) and hence the dialog failed to open.  This issue was fixed in NX 12.0.2. 

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Balloon size must be larger than 0

Master
Master
Thank you both. I got this fixed. The dlx file was like 45789kb. A little outa hand so hopefully that will help with my lag in NX?
Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Balloon size must be larger than 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

One can hope.