Cancel
Showing results for 
Search instead for 
Did you mean: 

Balloon status NX

Hello 

I have a problem I have almost 200 parts in an assembly

I have the part list and i put the balloons in the views

 

It is very difficult to Know wich Items have already the balloom 

and wich Items doesn't have it

 

Regards

8 REPLIES

Re: Balloon status NX

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

There is a journal posted in the following thread that may be useful:

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Auto-balloon-integrity-checker/m-p/3...

Re: Balloon status NX

Hello and Thank you cowski1

I saw a code but i don't understud

Where can I write the code?

Re: Balloon status NX

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Open a plain text editor (such as notepad) copy the code and paste it into a new text file. Save it somewhere you can easily find it later. Important: be sure to change the file extension from "txt" to "vb". In NX, go to menu -> tools -> journal -> play... and browse to your file then "run" it.

Re: Balloon status NX

Thank you but

It doesn't work 

"parts list callout column not found"

 

Some softwares offer an additional column which tell us
that information I think that is easier

I shared a picture

Re: Balloon status NX

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Your screenshot does not look like a standard NX parts list to me. Is that from NX or a spreadsheet? Are you using an add-on to NX such as moldwizard?

Re: Balloon status NX

It's another software which add an additional column which tell us
the information about the balloon status (It's only an example)

 

I share you an image wich shows the problem

Re: Balloon status NX

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

One of your parts list columns will need to be set to use the "callout". Select the column that you want to use for the callout, edit the settings, and select the "callout" option for the column category.

Re: Balloon status NX

Good¡¡¡

Thank you very much

Cowski1