Cancel
Showing results for 
Search instead for 
Did you mean: 

Bend angle's accuracy change ?

Genius
Genius

Hi

How to change bend angle's decimal accuracy?

Bend Angle = <!KEY=77692,3.2@UGS.angle>  (Where does it get its ".00" accuracy ?)

-> Note: Its someone else made drawing so it does not use my defaults...

 

TAITTO TOLERANSSI.png

2 REPLIES

Re: Bend angle's accuracy change ?

Phenom
Phenom

I don't use sheet metal at all, so I'm only guessing here...

But I think the "3.2" defines the way the number is displayed with the ".2" being the number of decimal places. So you could try changing that to "3.0".

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]

Re: Bend angle's accuracy change ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

I think i have tried it in the past but not sure....Will this help?

flat.jpg