Cancel
Showing results for 
Search instead for 
Did you mean: 

Bend angle still 2 desimals after changing customer defaults ?

Genius
Genius

Hello

Bend angle is still 2 desimals(,00) after changing customer defaults ?

- I exited already NX 9.0. Closed from "X".

- Do I need to restart computer to make it work ?

 

still 2 desimals.jpg

3 REPLIES 3

Re: Bend angle still 2 desimals after changing customer defaults ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
did you also update your part preferences?

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Bend angle still 2 desimals after changing customer defaults ?

Genius
Genius

I have only learned to change Customer Defaults.(Mine first 5 months with NX 9)

Where to find Part Preferences ? (Flat-Pattern's bend radius desimals)

Re: Bend angle still 2 desimals after changing customer defaults ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
go to file->preferences-> sheetmetal
in the tab callout configuration you can check if this is the same as the customer defaults.
and check also the Flat pattern display if the custom callout is set.

Some of the settings in the customer defaults are session settings and will work after restart.
Some of the settings in the customer defaults can be over ruled in your part preferences.
So these settings in de customer defaults you can see as a vault (database).

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions