Cancel
Showing results for 
Search instead for 
Did you mean: 

Bending and unbending tubing

Honored Contributor
Honored Contributor

I have a user, that is trying to model, bend, and then unbend a piece of tubing, using sheet metal module.  He wants the unbent form, so it can be laser cut, and the bent for use in the assembly.

 

he's had no luck, and I've tried to help, but because it's not true sheet metal, and bends and normal cut outs are 90° to each other, they don't play well together.

 

So far, my best solution is to model it unbent, extract a body at time stamp, and then bend the original into the finished shape.  I was actually surprised he got the "Bend" feature to work, on hollow tubing.

 

Is there a better tool, or module to do this?  Mechanical routing maybe?

 

UnBent.JPGBent.JPG

-Dave
NX 11 | Teamcenter 11 | Windows 10
37 REPLIES 37

Re: Bending and unbending tubing

Phenom
Phenom

May be my model will be useful.

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Bending-a-tube/m-p/427749#M15931

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Bending and unbending tubing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
@DaveK
do you have a movie of how you create this?
i'm trying to do this but in wont work.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Bending and unbending tubing

Honored Contributor
Honored Contributor

No, but I can upload the file.  You can see he started with a linked body, which was the original 3 piece tube, as reference.

 

I think you can follow the rest of his workflow.  The extracted body, was added by me, as a way to preserve the profile needed for laser cutting the tube with the notches.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Bending and unbending tubing

Siemens Phenom Siemens Phenom
Siemens Phenom

Dave I took your stock body and used split body and move face to get it into the final position. I have attached the part file. I will think about a way I maybe able to do this by starting with the finished shape to move it into the straight shape. 

 

Scott

Re: Bending and unbending tubing

Honored Contributor
Honored Contributor

Thanks.  It just seems like we can't the the only company that would notch, and bend rectangular tubing like this, so I figured there would be some method, or capability within NX.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Bending and unbending tubing

Phenom
Phenom

Since no favorable answer here for this simple task within NX, I just look how easy it could be with other software.

It took me 15 minutes  to build a model with parametic capablity. It may take another 5 minutes to get a drawing and a DXF file.

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Bending and unbending tubing

Phenom
Phenom

@AmyReyes ; 

I’m trying to insert videos in MP4 & AVI formats with the video upload (Camera Icon) function; but it isn’t working anymore. Could you please check?

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Bending and unbending tubing

Honored Contributor
Honored Contributor

I could download the videos, just not watch in the webpage.

 

That said, I could probably build a fully sheet metal file like that in NX, and get it to unfold, but ideally I'd like a tool that will bend/unbend rectangular tubing.  Getting the notches laser cut, and then folding, would seem to be a common industry practice.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Bending and unbending tubing

AmyReyes
Retired

Hi @mike_fdo

 

I am able to attach videos without issue using the camera icon. If you are using Internet Explorer, please check your browser settings. Compatbility View Settings must be unchecked/set to off.

compatibility view.jpg

That is usually what causes most of the issues you're describing. Let me know if this works, and if not, I'll continue to work with you to find a solution. 

 

Thanks!

 

Amy

 


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!