02-22-2017 05:37 AM
Hello
Where in Customer Defaults is:
Body Measurement: Change Area mm2 to m2 ?
02-22-2017 06:13 AM
Simply change the unit of part. Measurement information will be shown as per selected unit.
Regards,
Ganesh
#IngenuityIsNX | NX - What's New
02-22-2017 06:41 AM
Go to menu->analysis->units and set here the wanted unit.
if you changes this in you template everything will be using this unit.
02-22-2017 08:26 AM
Be aware that changing the analysis units as above will also change the default units for new sketches. For instance, changing the units to kg-m will result in meters being used as the length unit when creating sketch dimensions.