Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Bolt Circle Centerline in PMI

Siemens Phenom Siemens Phenom
Siemens Phenom

I am creating model using PMI so that it would be completely Model Based Definition.


I have created the center marks and a centerline using commands available within PMI application as shown in the attached image of this post.

Now I want to create Bolt Circle Centerline, Its available in Drafting application. I did not find such option in modeling application. One workaround will be create sketch and show it but this will not fulfill the MBD requirement.

Is there any way/command available so that I can create Bolt Circle Centerline in modeling application.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

1 REPLY

Re: Bolt Circle Centerline in PMI

Siemens Phenom Siemens Phenom
Siemens Phenom

NX12 will include a PMI Bolt Circle.