Cancel
Showing results for 
Search instead for 
Did you mean: 

Bolt Circle Centerline through 2-points (180° apart)?

Experimenter
Experimenter

I have 2 holes that lie on a common bolt circle. The holes are 180° apart on the circle. Is there a way to create a bolt-circle centerline through these two points?

 

The options that I see are:

 

   Through 3 or More Points (but we only have 2 points...)

 

   Center Point

 

I can create a point, between the two hole centers, and then use the "Center Point" option - but the created point doesn't appear to be associatively linked to the two holes.

 

What is best-practice for creating a bolt-circle-ceterline through 2 holes that are located 180° apart on a common circle?

 

Thanks,

Steve

4 REPLIES

Re: Bolt Circle Centerline through 2-points (180° apart)?

Legend
Legend

I would use 1 Center Mark with 2 center points. The linear distance between hole centers is the same as a theoretical diameter between them.

 

2 hole centerlines.PNG

-Tim

Re: Bolt Circle Centerline through 2-points (180° apart)?

Experimenter
Experimenter

Thanks. I realize that I can dimension the (2) holes as you've shown. I was looking to dimension them as shown below. I used a sketch to do this - but was looking for a method that uses the drafting-application's Bolt Circle Centerline functionality.LoadMe.jpg

Re: Bolt Circle Centerline through 2-points (180° apart)?

Siemens Phenom Siemens Phenom
Siemens Phenom

Create a sketch in the view and insert some helper geometry in the sketch to drive the bolt circle centerline and then hide the sketch.

 

(view in My Videos)

 

Regards, Ben

Re: Bolt Circle Centerline through 2-points (180° apart)?

Experimenter
Experimenter

Thanks Ben. I ended up basically doing what you showed in your video. That works fine for the desired result. I was thinking that a 2-hole bolt-circle was a common enough occurence that NX might have a built-in method for handling this. The logic could be;  if only 2 hole centers are picked - then use the midpoint between them as the center of the bolt-circle (possibly including a check-box for 2-hole situation) - or allow access to the point-dialog when in the command - so that the "between two points" option could be used to locate the bolt-circle center point.

 

I appreciate you including the video - that validates the method that I had used to get the desired result!

 

Steve