Cancel
Showing results for 
Search instead for 
Did you mean: 

Bookmarks NX10 with TC integration

Siemens Builder Siemens Builder
Siemens Builder

Hi experts!,

a costumer ask me about Bookmark info save when NX is integrated with Teamcenter.

The quetion is if Bookmark is saved in user sesion or bookmark is saved in a "common"

directory inside Tc.

They want to know also if bookmarks generated in a session in TC can be accesed

by any user in Tc that open the assy where the bookmark was generated.

 

Thanks in advanced.

2 REPLIES 2

Re: Bookmarks NX10 with TC integration

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @FidelM,

 

If I remember it correctly, bookmarks are only storred locally on OS level not in TC. So also sharing bookmarks umongst user can be done on OS level. Not in TC.

 

I hope this helps.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Bookmarks NX10 with TC integration

Genius
Genius

Dennis is right, Bookmarks are saved to the local file system whether you're in Native or Managed.

 

You could store them in Teamcenter, if you wanted to.  You could setup a new dataset type so that it lives with the part - though you'd have to export it out everytime you want to open it.  You could probably make this more seamless, but it would require some customization.