Cancel
Showing results for 
Search instead for 
Did you mean: 

Break multiple wave links at once?

Honored Contributor
Honored Contributor

NX9 Tc10

 

I know I've asked this before, and it wasn't available then...is there a way now?  Before we release a part, our policy is to break all the active wave links, and a single step would be a time saver.

 

Thanks,

 Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10
5 REPLIES

Re: Break multiple wave links at once?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Write a journal?

If you have a release procedure, this could probably be incorporated in that so you don't depend on users doing it.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Break multiple wave links at once?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Forgot to mention...

You could also look at freezing the WAVE link (this prevents updates from happning, but later if you DID want an update, you just have to un-freeze - no need to re-link or anything like if it is broken)  I think it is also better at preserving the "where did I come from" info about the WAVE link feature.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Break multiple wave links at once?

Phenom
Phenom

This freeze option, what version of NX was this first introduced?  THanks

 

Re: Break multiple wave links at once?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The freeze and thaw options have been around for quite some time, but I'm pretty sure that you need the advanced wave control license (or whatever it's called) to use these functions.

Re: Break multiple wave links at once?

Honored Contributor
Honored Contributor

I need to look into this link freezing.  Thanks.

-Dave
NX 11 | Teamcenter 11 | Windows 10