Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Breaking dimension lines NX9

Experimenter
Experimenter

Hi all

 

I have move recently to NX9 (previously I worked with Catia V5 several years). When drafting, I can not find how to break a dimension line, I tried settings ->Line/arrow->Break but it doesn't exist in NX9, or I am not able to find it.

 

Just in case, I am referring to breaking dimension lines like in the attachment.

 

Thanx in advance

 

 

6 REPLIES 6

Re: Breaking dimension lines NX9

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Alot ,

Automatic line breaks was introduced in NX 10.

Re: Breaking dimension lines NX9

Experimenter
Experimenter
And is there any way to break the lines manually?

Re: Breaking dimension lines NX9

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Alot ,

 

Please refer below link for the same:

 

BREAK EXTENSION LINE

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Breaking dimension lines NX9

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

This can be achieved in NX9 using user defined symbols

 

Menu->Insert-> Symbol->User Defined-> Select any of the GAP type-> Select Add to drafting object button->Select the dimension to which the gap needs to be added->Click on standalone symbol button->Pick the desired location

 

Refer attached AVI.

 

Regards,

RahulC

Re: Breaking dimension lines NX9

Experimenter
Experimenter

Thank you so much.

 

Quite tedious method but seems to be the only one. In my opinion, a remarkable defect on NX9.

 

Anyway, thanks for the answer, very useful for me.

Re: Breaking dimension lines NX9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Alot wrote:

Quite tedious method but seems to be the only one. In my opinion, a remarkable defect on NX9.

 


Welcome to 2013. If you are stuck on NX 9, there is a journal here that will remove most of the tedium of placing dimension breaks.