Cancel
Showing results for 
Search instead for 
Did you mean: 

Bridge surface

Builder
Builder

Hello,

 

I'm trying to create a radius between 2 surfaces on a 3D-impeller.

 

I created the 2 surfaces, they're seperate from eachother. But I need to connect them at the top with a smooth radius. I used a bridge surface to do so.

 

2018-02-01 13_13_52-NX 11 - Modeling - [LaufradSurfaceModeling.prt (Modified) ].jpg2018-02-01 13_12_17-NX 11 - Modeling - [LaufradSurfaceModeling.prt].jpgEverything is fine so far. But when I extend the sheets, so they can be trimmed on the hub/cover plates.. the surface bridge comes loose from the other created surfaces:

2018-02-01 13_18_41-NX 11 - Modeling - [LaufradSurfaceModeling.prt (Modified) ].jpg

The bridge surface is created on sketched, straight lines. As are the connecting surfaces.

 

 

Is this not the right method to achieve what I need, or should I use a different feature perhaps? Any tips are welcome.

 

Edit: To clarify -> I need the surfaces to connect together so I can create a solid body out of it.

4 REPLIES

Re: Bridge surface

Genius
Genius

Try making the solid first and then using a face blend three face. Attached is a example prt. This is what I have done in the past.

Kurt Neubaecker
CAD/CAM Designer
Proficient Industries
Cleveland, Ohio

Re: Bridge surface

Builder
Builder

Hi,

 

I can't open your file because it's from a newer version of NX than what I'm currently on.

Re: Bridge surface

Genius
Genius

Here is a quick video. What version of NX are you using?

Kurt Neubaecker
CAD/CAM Designer
Proficient Industries
Cleveland, Ohio

Re: Bridge surface

Builder
Builder

Thank you for the video. That looks super easy! I will try that.

 

 

I'm on NX 11.0.1

 

 

Edit: Worked like a charm! Thank you!