Cancel
Showing results for 
Search instead for 
Did you mean: 

Can I make the pitch visible from a threaded hole.

Valued Contributor
Valued Contributor

Can I make the pitch visible from a threaded hole,I can make it visible with a bolt

5 REPLIES 5

Re: Can I make the pitch visible from a threaded hole.

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

Is it a drafting application?
Is it a dimension?

 

If so, HoleCallout will display the pitch.

Please tell me more detailed information.

 

pitch.png

Re: Can I make the pitch visible from a threaded hole.

Valued Contributor
Valued Contributor

It is a partPart1.png

Re: Can I make the pitch visible from a threaded hole.

Siemens Phenom Siemens Phenom
Siemens Phenom

For existing threaded hole (created using the hole command), it is not possible. You have to create a simple hole first, then use 'Thread' command with thread type as 'Detailed'.

Re: Can I make the pitch visible from a threaded hole.

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

The hole command does not represent a detailed thread shape.
Use the Tread command for a simple hole.

 

Thread_detail.png

Re: Can I make the pitch visible from a threaded hole.

Valued Contributor
Valued Contributor

Thanks, it works