Cancel
Showing results for 
Search instead for 
Did you mean: 

Can You Copy An Explosion To An Arrangement?

Experimenter
Experimenter

Hi All,

 

Simple question really, can the exploded layout be copied to an arrangement?

 

We've a designer here who has completed a large task of creating views and has used the exploded view commands. Trouble is the JT viewing program we use here can't see the exploded view however it can see arrangements. He's completed around 30 assemblies so a quick fix would be nice!!

 

Thanks

5 REPLIES

Re: Can You Copy An Explosion To An Arrangement?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Quick answer: No, an exploded view cannot be copied to an arrangement.

Re: Can You Copy An Explosion To An Arrangement?

Experimenter
Experimenter
That's what I was thinking!!

Just thought I'd ask the experts here in case I was missing something.

Thanks for the quick confirmation cowski1 :-)

Re: Can You Copy An Explosion To An Arrangement?

Gears Phenom Gears Phenom
Gears Phenom

We have done all of our explosions as arrangements in NX.  We do not use the Explosion function do to explosions and arrangements not working with each other. 

 

 

Re: Can You Copy An Explosion To An Arrangement?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Paul_Nissan,

Exploded views gets stored in JT file as part of the PMI data and it can be seen in the Teamcenter Visualization. Also in free viewer JT2GO which is again based on the TCVis.

 

Regards,
Ganesh

Re: Can You Copy An Explosion To An Arrangement?

Experimenter
Experimenter

Ah that could be a way around our problem - I'll investigate.........

 

Thanks