Cancel
Showing results for 
Search instead for 
Did you mean: 

Can a user define the toolbar menu tabs to be left justified in the interface?

Creator
Creator

When customizing an interface layout, the toolbars would snap into a left justified position on my screen. With a new installation of NX 11 it appears that the toolbars are now justified to the center of the interface. I prefer to have the tabs left justified.  Can this still be done? Here is a snapshot. Why is my 'File" menu the only one that is to the left?Menu Bar.PNGCan I move all my buttons to the left?

2 REPLIES

Re: Can a user define the toolbar menu tabs to be left justified in the interface?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @LouisP,

Menu > Preferences > User Interface (Ctrl+2)

Select 'Layout' and make sure that option 'Slim Ribbon Style' is unchecked.

 

Ribbon_Style.png

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Can a user define the toolbar menu tabs to be left justified in the interface?

Creator
Creator

Excellent! Thank you, that solved the issue.