Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not attach two sketches together NX 11

Creator
Creator

I am making a fuselage and the problem is that i can not put the points from the scetch 1 to scetch 2. Picture better describe my problem. In Solidworks there is an option, called "pierce", is there the same one in NX or other option? Thank you for your answer Снимок.JPG

7 REPLIES
Highlighted

Re: Can not attach two sketches together NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom
Check if Project curve is useful in your case depending upon the plane used for the sketch.
Menu > Insert > Derived Curve > Project.
Regards,
Ganesh

Re: Can not attach two sketches together NX 11

Creator
Creator

It does not help. I need to connect points from scetch 1 to scetch 2 and 3, as in this video https://youtu.be/VVfCIuub7XA?t=15m39s

Re: Can not attach two sketches together NX 11

Pioneer
Pioneer

You need to make intresected (line - datum plane) points in scetch#1 and then use them in scetch#2.

Like SolidWorks don't work in NX


Сhannel for NX users (Russian language) https://www.youtube.com/channel/UCvf0Rp4Sy6bRRyTYBF9rnJQ

Re: Can not attach two sketches together NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Sorry i know you have already accepted the solution but doesn't INTERSECTION POINT within sketch is the answer you are looking for?? 

(view in My Videos)

Best Regards

Kapil

Re: Can not attach two sketches together NX 11

Creator
Creator

Hi, Kapil!

Yes, that is the way I do it now! Valeo-ua in the previous message said exactly the same thing) Thank you for your reply!

 

Regards

 

Andrew

Re: Can not attach two sketches together NX 11

Pioneer
Pioneer

Your way is also right. but...
but sketch1 = 1 position
sketch1 + intersect = 2 position (minimum)


Сhannel for NX users (Russian language) https://www.youtube.com/channel/UCvf0Rp4Sy6bRRyTYBF9rnJQ

Re: Can not attach two sketches together NX 11

Pioneer
Pioneer
attached: your option is only using when the section planes doesn't perpendicular to plane of sketch.

Сhannel for NX users (Russian language) https://www.youtube.com/channel/UCvf0Rp4Sy6bRRyTYBF9rnJQ