Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not import part file into STAR-CCM+

Experimenter
Experimenter

Hi,

 

I have a simple 3D CAD model with different parameters defined as expressions, such as 'Chamfer Offset' and 'Extrude End Limit'. This is done to perform an optimazation study in STAR-CCM+. Everything works out with exporting in Simcenter NX but when I import the .prt file as 3D model I get the following error: 

 

Error during CAD import. Details in log file D:\...\Block.prt.log

 

With the following details in the log file: 

Command line : --input D:\Block.prt --output C:\Users\student\AppData\Local\Temp\661d1814-5282-424b-a5e6-3259737d6378.x_t --parasolid_pass_through --logfile D:\Block.prt.log 

HOOPS Exchange 10.2
64-bit Unicode
PK 30.0.269
ERR LoadFromFile Error -10005 D:\Block.prt

 

If I export the CAD model into a .STL, .STEP or .x_t it works fine but then I am losing my parameters which is the most important part of my design. Help is really much appreciated, thank you!

 

Regards, Revrask2

2 REPLIES 2

Re: Can not import part file into STAR-CCM+

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would look in D:\Block.prt.log to see if any more (or more specific) errors.

I'm not sure about Star-CCM+, but in general, all the translators will remove the parameters and end up with a "dumb" solid (parameter passing is not part of the spec for the neutral formats)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Can not import part file into STAR-CCM+

Experimenter
Experimenter

Thank you for your reply.

 

Unfortunately, this is all the information given in the log file. So there is no more explanation of the errors..

 

I get your statement about parameters and 'dumb' solids. I would like to run an optimazition inside STAR-CCM+ Heeds to improve my design with parameters defined in NX (Simcenter).. 

 

It is possible to make different designs in NX and export as .x_t although it should also be possible to export as .prt from NX to import in Star. I do not know where this error is based on.. Thank you anyways!