Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not save file

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Deal all

 

I am using NX 10.0.2.6 MP1 . I have create model and cam process. when I am finishing I have to save file but NX does not save. It show no part file save . How to solve it ?

 

Thank you 

 

2 REPLIES

Re: Can not save file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

File -> Save -> choose one of the save options?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Can not save file

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Do you mean that you do not have any Save options on the menu under File?

 

If that is the case, you may be running a custom menuscript file where the Save options have been removed or hidden.

 

Check with your system administrator if that is the case.

 

If it is something else, please explain in detail to help us understand the problem.  Thanks!