Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Creator
Creator

I can't create a new project on mold and no find any Standard library on  MW Mold Base Library . Please help me. I installed Excel...123.jpg

7 REPLIES 7

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

It sounds like you need to download and install the data files for Moldwizard.  From the product download server, select "NX > Product Updates > Moldwizard > Nx11" and you'll find:

  • mwnx11.0_data.README.txt
  • mwnx11.0_data.zip

You may also need to set MOLDWIZARD_DIR as explained here in the documentation.

 

Regards, Ben

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Creator
Creator

I install Moldwizard the same way file : " mwnx11.0_data.README.txt " but i can't do that , when i create new project , on Assembly Navigator not have appear all file assembly for Mold Base

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

It appears that NX is not reading the moldbase_reg_mm.xls file in %MOLDWIZARD_DIR%\moldbase\metric\
First check that the moldbase_reg_mm.xls file exists in the above directory.

 

If the file exists, try manually adding the Moldwizard Add-In to Excel.  From an Excel session (with a blank file open), select "File > Options > Add-Ins" and at the bottom of the page select the "Go" button for "Manage: Excel Add-Ins".  Hit the Browse button and navigate to %MOLDWIZARD_DIR%\templates and select moldwizard_add_in.xla.  Choose OK, make sure the Add-In is checked, and choose OK again.  Restart NX and see if the DME folder now contains mold bases in the Member Select window.

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Creator
Creator
I Need •mwnx11.0_data.zip
From where I can download •mwnx11.0_data.zip ??
I Can't found the download link/Page as above mentioned ("NX > Product Updates > Moldwizard > Nx11")

Can u please share me the Download link.?

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Siemens Phenom Siemens Phenom
Siemens Phenom

It can found at the Download and Upload files link from the GTAC page. That page is here:

 

GTAC Home Page

 

Thanks,

Scott

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Creator
Creator

I did but have a problem on the picture

17474217_706765282818411_2034599933_o.png

Re: Can not to create New Project and Install Moldwizard Library on MOLD TOOL

Creator
Creator
Who can help me ?