Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not unfold this part in UG nx 11 ,please help

Experimenter
Experimenter

I have tried all the possible method to unfold attached part using analyze formability(one-step),please someone can fix it and let me know how to get a a unfold sheet,thanks very much.

5 REPLIES 5

Re: Can not unfold this part in UG nx 11 ,please help

Valued Contributor
Valued Contributor

I copied the body (1) into new sheet metal part, and after "Convert to Sheet Metal" cmd with setting "Preferences for sheet metal" thickness=1mm, I could make a Flat Pattern and Unbed the part like this:

 

flat pt.png

 

But the Convert takes a lots of minutes Smiley Wink. Could it be a solution for you?

 

The part is attached:

 

Re: Can not unfold this part in UG nx 11 ,please help

Valued Contributor
Valued Contributor
One more thing...The inner radius is only 0,08mm, If you want to bend it you should increase it. I think for 1mm thicknes is r=1mm, but I'm not sure of the exact numbers. :/

Re: Can not unfold this part in UG nx 11 ,please help

Experimenter
Experimenter

Thanks very much,it indeed can solve the problem for some of my parts. I have a project with may parts like this,but most of the parts still can not be unfold,it reminds the following information when i try to convert to sheet metal part,because the part itself is a solid,i don't know what do do about this,i also try to create a midleface,sew them together, trying to unfold using one-step analysis,but still no luck...it would be apprecaite if you could take more time to check this part for me.111111111.png

 

Re: Can not unfold this part in UG nx 11 ,please help

Siemens Phenom Siemens Phenom
Siemens Phenom

Can I ask how these parts were created?  For a valid sheet metal part, the material must be a constant thickness.  Convert to Sheet Metal can convert most things and in some cases cleanup and/or optimize face are needed before converting.  Take a look through the part and see if it can even be manufactured.  for example, this area would be a challenge and may be the cause of Convert not allowing flattening.

Picture1.png

 

See if you can adjust the geometry to get the following profile before trying to convert

2017-08-29 08_39_21-NX 11.0.2.7 - Sheet Metal - [sheet_metal_model4.prt (Modified) ].jpg

 

Have a look at the attached.  You'll note some areas have been removed - they would need 'fixing' too.

Re: Can not unfold this part in UG nx 11 ,please help

Experimenter
Experimenter

thanks for the reply and advise,now i know how to fix them now.