Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't see overall object

Creator
Creator

As the title, I can't see the overall object when I design in NX 11. This problem just occurs when I set dimension over 1000mm. Please help me fix it.

(view in My Videos)

4 REPLIES

Re: Can't see overall object

Phenom
Phenom

That is caused by the clipping planes. @GaneshKadole explains it pretty well here:
Clipping Planes

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]

Re: Can't see overall object

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Performing a view fit will reset the view clipping planes based on your objects (right click -> fit, or Ctrl + F, or menu -> view -> operation -> fit).

Re: Can't see overall object

Siemens Phenom Siemens Phenom
Siemens Phenom

A fundamental understanding of Cameras will help you realize why your clipping planes are chopping off your geometry in the view.  Take a few minutes to read the documentation on cameras and the controls and play around with the settings; adjust the clipping planes in the view and drag the handles on the Target and Camera CSYS - it should all become clear why your graphics window displays the way it does.

 

Regards, Ben

Re: Can't see overall object

Creator
Creator

Thank you for your help. I did it