Cancel
Showing results for 
Search instead for 
Did you mean: 

Cant change ratio of my drawnigs in drafting mode.

Experimenter
Experimenter

Hello, i need to make a draft with the top, front and right view and when i do the draft the three faces if the draw are very very small, i tried to change the ratio of the front and top view to 1:1 and they just simply dissappear and when i change the ratio of the right face to 1:1 it changes without problem.

1 REPLY

Re: Cant change ratio of my drawnigs in drafting mode.

Gears Phenom Gears Phenom
Gears Phenom

Review the location of your View anchor point.  Sometimes NX takes a good guess at this location.  you can change this view Anchor point to a central point and try updating your views.  Just a thought