Cancel
Showing results for 
Search instead for 
Did you mean: 

Chamfer behaviour

Gears Phenom Gears Phenom
Gears Phenom

Ciao,

 

excuse me for the trivial question, someone can explain to me why this different behaviour of the Chamfer command?

 

Grazie

 

chamfer.png

2 REPLIES 2

Re: Chamfer behaviour

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Cesare,

 

The behavior is based on the trimming (and attach) rules built into the feature. The rule is as the all the edges comes together as in the example the chamfer is also applied to the “vertex” or resulting edge. The same actually goes for blending, but you probably don’t even reflect over it.

 

Best Regards
Fred

 

chamfer_triming.JPG

Re: Chamfer behaviour

Gears Phenom Gears Phenom
Gears Phenom

Ciao @Sandman,

 

you are right, I don't reflect over blend. It means that there may be other solutions for the Chamfer as for the Blend. Very interesting.

 

Grazie