Cancel
Showing results for 
Search instead for 
Did you mean: 

Change default in Weld Symbol > Weld Line

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi

 

Does sombody know if there are some workaround in NX, which can be used to change the default Weld Line type from "Plain" to "ID line Above".....

As I can see , the only way is to save menu layout as favorite, and then call it from a custom command....

Is this the way to do it ? and in a global setup with many users , as well?

 

regards Lars

2016-08-23 15_26_50-NX8.5 for Siemens Wind Power - Drafting - [LayerOrganizer.prt (Modified) ].png2016-08-23 15_27_07-NX8.5 for Siemens Wind Power - Drafting - [LayerOrganizer.prt (Modified) ].png

2 REPLIES

Re: Change default in Weld Symbol > Weld Line

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Why would you have to call it from a custom command?

After you save a favorite, you can start the command normally then click the gear icon in the upper left corner and select your favorite from the list.

Re: Change default in Weld Symbol > Weld Line

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi cowski - thanks for your reply...

I was not aware about, (or has forgotten) that dialog remembers user favorites after restart of NX...

So you are right - it shouldnt be nesseary to create a custom command .....

But if I save the favorite in Site Level, I hope it will be the default dialog for all users afterwards in their sessions..If not - maybe a global custom command is needed anyway...

 

Lars