Cancel
Showing results for 
Search instead for 
Did you mean: 

Change edge color in Static Wireframe View

Valued Contributor
Valued Contributor

Hey friends,

i need to change edge color in static wireframe view.  Because it's looking like faded colors.

i found change menu in costumer default. 

But it doesnt work , can not choose color. 

 

i will appreciate if someone tell something.

Best regards,

Alican

 

 

 

edge color.png

 

8 REPLIES

Re: Change edge color in Static Wireframe View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The edges in static wireframe view inherit the body color.

Re: Change edge color in Static Wireframe View

Valued Contributor
Valued Contributor

thank for answer friend.  i know this but i need to change .

Re: Change edge color in Static Wireframe View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Then you will have to change the color of the body.

 

The faces can have a different color from the body so that it appears one color (the face color) in shaded mode and another color (the body color) in the static wireframe display mode.

Re: Change edge color in Static Wireframe View

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi buddy,

 

Go to Preferences -> Object -> General

under "Type", select solid body, select the color that you want. .

create a solid body and then apply the static wireframe view . .

it should adapt the color that you selected.

you can also set this as default body color in the customer defaults.

Go to Customer defaults -> Gateway -> Object , then go to solid body tab.

there you can change it's color. .

 

hope this helps. .

 

Regards,

Sen

Re: Change edge color in Static Wireframe View

Valued Contributor
Valued Contributor

hey friend ,

Thank you for your help.  I know when we change body color , it adapt the color in static wireframe view.

But i dont need this. I need only change colors in static wireframe  when body color is same.

i found some setting in visualization preferences  at NX 10.0.1.mp3 ,but it doesnt working . It doesnt let to choose line color in wireframe or static wireframe.

 

 

 

2015_06_11_10_28_39_NX_10_Modeling_3382011622_B_2_stp.prt_Modified_.jpg

Re: Change edge color in Static Wireframe View

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

 

What Cowksi mentioned is the only way to do what you're after.

The setting you've mentioned for 'Shaded Edge Colour' is exactly what it says, the colour of an edge in a 'SHADED' view. A Wireframe view is NOT shaded.

 

Look at the video attached to see what Cowski is referring to.

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Change edge color in Static Wireframe View

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

The option you are showing us will just change the color of the edge of the solid body, it is located in the customer defaults under gateway - > visualization - > visual but it has no effect in the color of the edges when rendering in static wireframe, since the edge color in Static Wireframe only adapts the color of the solid body itself.

 

you can try this but it will take your time a bit.

 

  1. create a model (default color of the body)
  2. change the color of the body (to the desired color in static wireframe)
  3. in the selection filter choose face and change the color of all the faces of your model (back to the color of the default body)

now, you have your default body color in shaded view and when you view your model in static wireframe, it will adapt the body color.

 

 Regards,

Sen

 

Re: Change edge color in Static Wireframe View

Valued Contributor
Valued Contributor

Thank you friend.