Cancel
Showing results for 
Search instead for 
Did you mean: 

Change interface to classic toolbars in NX 11

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

how I can change interface to classic toolbars in NX 11. I am not able do that in the same way as in prevoius version of NX. I've heard that I can to that by some envirement variable but I don't know which one. Are you able to help me??

 

best regards!

lukipap

6 REPLIES

Re: Change interface to classic toolbars in NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

File > Preferences > User Interface (Ctrl+2)

 

Layout > User Interface Environment > Select the 'Classic Toolbars'

 

toolbar.PNG

 

Re: Change interface to classic toolbars in NX 11

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

In NX11 this function has been removed. Only in NX10 it has been available

Re: Change interface to classic toolbars in NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: Change interface to classic toolbars in NX 11

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
The command Finder will be your best friend in the beginning.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Change interface to classic toolbars in NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no option or any other way to turn on the classic toolbars staring in NX 11. The ribbon bar is the only interface moving forward as of now.

 

Scott

Re: Change interface to classic toolbars in NX 11

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

One hint I give our users - use the "border bars" around the graphics screen.

E.g. if you have you "navigator" windows to the left...

Any button you regularly use that is NOT on the "Home" tab for the application, add it to the "left" border bar (Right-click on icon -> Add to XXX border bar.  If you can't find an icon to do this, use command finder to find the command, then in command finder "results" window: Right-click on icon -> Add to XXX border bar)

Note border bars are application specific!

First ones I do are the "other" applications you use (e.g. in modeling, I add drafting & manufacturing)

Next ones are layer control & Info object

I do a lot of work on post processors, so I add the "Log file" (to debug when post dies)

Others as appropriate for the way you use NX.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled