Cancel
Showing results for 
Search instead for 
Did you mean: 

Change the numbers in BOM

Pioneer
Pioneer

Hi

 

It is possible to change the number  in PC NO in BOM. I want to use the Alphabets instead of numbers..

3 REPLIES 3

Re: Change the numbers in BOM

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes.

Native or managed NX? Is there any specific purpose to use alphabets instead of numbers?

Highlighted

Re: Change the numbers in BOM

Pioneer
Pioneer

HI,

 

Not like that just , i need information about that. How it is ?

Re: Change the numbers in BOM

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @S7

 

Right click the top left corner of the Parts List and choose Settings.  With Parts List selected in the menu, scroll down to find "Initial Callout" and change it from "1" to "A".  Close the dialog and the Parts List should now show letters instead of numbers.

 

Screenshot - 7_6_2018 , 7_58_52 AM.png

 

Does that help?

Regards, Ben