Cancel
Showing results for 
Search instead for 
Did you mean: 

Change unit of THREADED HOLE

Creator
Creator

Hello,

 

is it possible to change the unit of inch threads?

If I choose a Inch thread the diameter and the depth is changing to inch but it would be much easier for me to have this in mm

Thanks for your help!

MartinThread.jpg

3 REPLIES 3

Re: Change unit of THREADED HOLE

Honored Contributor
Honored Contributor

Type in the millimeter number, with mm behind it, ie 19mm.  NX will do the conversion.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Change unit of THREADED HOLE

Creator
Creator
I didn`t think that it would be so easy :-)
Thank you Dave!

Re: Change unit of THREADED HOLE

Honored Contributor
Honored Contributor

That will work with mm, ft, in, etc.

 

https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#uid:ui_use_uiu_num_convert_r

-Dave
NX 11 | Teamcenter 11 | Windows 10