Cancel
Showing results for 
Search instead for 
Did you mean: 

Check Surfaces Quality

Creator
Creator

Hi there,

 

I would like to check the quality of some surfaces, maybe its see if the U and V's are okay. Because i want to use Global Shaping after with the surface created, my objective it's avoid some deviation when i planificate some object.

 

I'm sending an image from ZW software, where the face quality is checked.

 

Face Quality.PNGThe red dots are the surface control points.

3 REPLIES 3

Re: Check Surfaces Quality

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Juks10 ,

 

You can try Face Curvature Analysis tool.

 

(view in My Videos)

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Check Surfaces Quality

Siemens Phenom Siemens Phenom
Siemens Phenom
when you say check quality, what is it you want to do ?
Surface quality can be measured / determined in many ways, one way is by studying the points/pole structure.
( which appears to be what's done in the attached image.)
if so, analysis - Show poles and / or Analysis - Show points

Regards
Tomas

Re: Check Surfaces Quality

Siemens Phenom Siemens Phenom
Siemens Phenom

Section Analysis - Uniform - Isoparametric

Can select U and V direction and the number of UV lines.

 

Steve V