Cancel
Showing results for 
Search instead for 
Did you mean: 

Check mate - Check nr. of solid bodies

Experimenter
Experimenter

I would like to use check-mate. I know it's possible to get information about how many entities thera are on a certain layer. I would like to edit that check and create a new one: 

Check passes when there is 1 solid body on layer 1 and

Check fails when there are 2 or more solid bodies on layer 1 and

Check gives a warning in case there is no solid body on layer 1

 

I would really appriciate it when someone could help me or even could send a *.dfa file!!

I am using NX 10. 

2 REPLIES 2

Re: Check mate - Check nr. of solid bodies

Experimenter
Experimenter

I didn't get any reply on my question. Is there anyone who can help me?

Re: Check mate - Check nr. of solid bodies

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Please take a look at existing Check-Mate template checker "Check if Layers Contain Objects of Valid Types" as example. The DFA file can be found in %UGII_BASE_DIR%\design_tools\checkmate\dfa\template\mqc_check_layers_objects_mapping.dfa. 

 

What you need to do is:

- copy this dfa as your own dfa, and update the display name, category etc.

- change the rules inside "check_rule" method to be the logic that you described. 

- put your DFA in Check-Mate search path (e.g. UGCHEKCMATE_USER_DIR).

 

Yunfei