Cancel
Showing results for 
Search instead for 
Did you mean: 

Check mate error - Check Annotations

Pioneer
Pioneer

Hello All,

 

I have tried to use the check mate node "Spell Check on Annotations" and got some weird results.

 

I changed the check mate settings to check only the "Notes" , and enabled "Show Spelling Tips" to find the correct spelling.

 

One of the note I had in my drg is
"ONLY ITEMS DESCRIBED ON THIS DRAWING ARE APPROVED FOR USE IN THE APPLICATIONS SPECIFIED  HEREON."

After running the checkmate it gives the following error log . (Attached )

 

Does anyone know what is wrong here ?

7 REPLIES 7

Re: Check mate error - Check Annotations

Siemens Phenom Siemens Phenom
Siemens Phenom
Unless you actually are running MSword 2003, turn of that option in the Customize test dialog box.

If you have a Title Block on the drawing, the text in it will also be checked. It appears that you may have a scale or units value of 'IN', which I suspect represents 'inches'.

Re: Check mate error - Check Annotations

Pioneer
Pioneer

Thanks for the reply,

I'm pretty sure that there is no such word acronym for inch.

It shows me the same error for "All DIMENSIONS ARE IN MM U.O.S" even after turning the check box"Check with custom dictionary only" off

 

Re: Check mate error - Check Annotations

Siemens Phenom Siemens Phenom
Siemens Phenom

To get the "All DIMENSIONS ARE IN MM U.O.S" to pass, you need to remove the periods '.' in the U.O.S.

Re: Check mate error - Check Annotations

Pioneer
Pioneer
Thanks, But the error log is on the "IN"
Suggested words are "INN", "INK", and "I."

Re: Check mate error - Check Annotations

Siemens Phenom Siemens Phenom
Siemens Phenom

A bit odd, as the word "IN" is actually a word in English.  (See what I did there?)

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Check mate error - Check Annotations

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does case matter?
"in" != "IN"?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Check mate error - Check Annotations

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Of course, "IN" is the postal abbreviation for Indiana!

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled