Cancel
Showing results for 
Search instead for 
Did you mean: 

Close gap between edges

Phenom
Phenom

Hi,

which is the best workflow or command to close this open (closed) sheet body ?

Attached the part.

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

2 REPLIES

Re: Close gap between edges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use "examine geometry to find the gaps (hint: it is a blend face on the +Y side of the body). Use the "unsew" command to remove this face from the body, then "sew" it back (use the default tolerance). A solid body will result.

 

Optional: use "optimize face" to clean up some of the geometry.

Re: Close gap between edges

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
What format was the original geometry? If it was an IGES or STEP both the IGES and STEP translators have the options: "Automatic Sewing of Surfaces" and "Sew Surfaces Automatically" respectively, that will create the solid body for you.