Cancel
Showing results for 
Search instead for 
Did you mean: 

Closing a displayed part contained in an opened assembly without keeping changes

Genius
Genius

What is the best practice for doing that?

4 REPLIES 4

Re: Closing a displayed part contained in an opened assembly without keeping changes

Creator
Creator

If you had modified the part ,Simply try closing the window,It will give three options 1. Yes-Save & Close 2. No-Close 3. Cancel  . select the second option.

Re: Closing a displayed part contained in an opened assembly without keeping changes

Genius
Genius

I think it doesnt work that way in NX 11.0.2. I think it doesnt ask me because if opened in an assembly the part is not really closed, which I prefer because the old behaviour was really annoying (part was closed and I needed to reopen it in the assembly context). Just a way to abort changes at closing displayed windows would be a plus!

Highlighted

Re: Closing a displayed part contained in an opened assembly without keeping changes

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you check, File > Close > Close and Reopen Selected Parts.

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Closing a displayed part contained in an opened assembly without keeping changes

Genius
Genius

I think that will work. Thank you Ganesh_Kadole!