Cancel
Showing results for 
Search instead for 
Did you mean: 

Color for "lost" fillet edges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Had a user ask, couldn't find anything.

- user fillets part

- then earlier feature is edited, and one or more filleted edges "goes away"

- User can edit fillet feature, and "lost" edges are shown "dashed", but in same color as rest of stuff displayed, so you have to really work to find them all.

 

Is there a way to get the edges that are shown as "dashed" to show as a different color as well?

 

Currently using 10.0.3

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


1 REPLY 1

Re: Color for "lost" fillet edges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Customer defaults -> modeling -> general -> miscellaneous -> diagnostics; it is a session setting.

 

Note that if you are happy with the resulting blend, you can quickly remove the lost edges by using "edit with rollback" and pressing the black X button in the select edge step then OK the dialog.