Cancel
Showing results for 
Search instead for 
Did you mean: 

Combining Parts into one single part in NX 10

Creator
Creator

Hey guys,

 

using NX 10 I've been trying to figure out how to use the Unite Command to combine a couple of parts into one single part in my Assembly, but for whatever reason when I want to "Select Body", I can't click on any of my parts to combine them. 

 

I also can't find a solution on the other forums, any ideas??

 

Connor 

5 REPLIES 5

Re: Combining Parts into one single part in NX 10

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I guess that your solid bodies are in separate parts.

Unite works with the selection scope: "Within Work Part Only"

Bodies to be united needs to be in the same part.

Re: Combining Parts into one single part in NX 10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Use wave link to promote the bodies to the assembly level and that unite them there.
Here is it possible to use the associative on or off. This will keep or remove the direct update link to the original body/part. (see settings in the wave geometry linker dialog)
Now all the bodies are in different part files.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Combining Parts into one single part in NX 10

Creator
Creator

I was able to do this, but I'm curious about what this actually does. From what I've read, using Unite allows me to literally connect the parts to a seemless connection. I'm using this to analyze my new assembly as one single part, but it isn't actually making that connection like I want it to. 

 

I want to parts that I originally have as an assembly to be one single  seemless part that can be analyzed with one fixed constraint and its forces.

Re: Combining Parts into one single part in NX 10

Creator
Creator

I've found a solution that works!

 

I tried lots of things while focusing on the "Unite" approach. The approach is outlined by JohnRBaker in this link:

http://www.eng-tips.com/viewthread.cfm?qid=261648 


Thanks to everyone!

 

Re: Combining Parts into one single part in NX 10

Gears Phenom Gears Phenom
Gears Phenom

Above link has a space at the end and results in a 404 error message.

 

Corrected link here -> http://www.eng-tips.com/viewthread.cfm?qid=261648

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1