Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Command Line Arguments for, Step, Dwg, and Iges

Innovator
Innovator

Is there documentation somewhere the details what the command line arguements / syntax would be fore creating Step, Dwg, and Iges files?

2 REPLIES 2

Re: Command Line Arguments for, Step, Dwg, and Iges

Legend
Legend

I dont aware of command line utitlity, but you can write a automation program to do this. 

 

Following may help

 

Exporting JPEG

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=export&dt=nx-api&file...

 

export pdf of each drawing sheet

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=export&dt=nx-api&file...

 

 

 

:Smiley SurprisedPTIMUS_PRIME

伊尔凡

Re: Command Line Arguments for, Step, Dwg, and Iges

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @InternBL,

 

Documentation:

Run translator from the command line (IGES only example)

Running translators from the command line (IGES and STEP example)

 

For example: $%UGII_BASE_DIR%\iges\iges.cmd ”D:\Iges\Solid.prt” o=”D:\temp\Solid.igs” d=”D:\iges\igesexport.def” l=”D:\temp\iges_log.log”

 

If you open the cmd file in a text editor you can see which options are available (o, l, d).  You'll also have to ensure that you're pointing to a valid JAVA install.  The docs do not appear to have a DXF example, however, if you review the 'dxfdwg.cmd' file in a text editor you'll see that similar options are used.

  

Note: Make sure you specify ".cmd" in the syntax to prevent the ".exe" with the same name from being used.

 

Regards, Ben